Cummins Guidanz DTK
Training home
Work with an engine / Advanced Features

Advanced Features

Review advanced features implemented in DTK and supported by the connected engine calibration.

Supported Advanced Features (PDF)

Compare support for DTK Mobile and DTK Windows. Availability depends on the connected engine calibration.

Expected result

The Advanced Features screen displays features implemented in DTK and supported by the connected engine calibration. Selecting a feature opens its screen and feature-specific instructions.

Important notes / prerequisites

Each individual Advanced Feature includes its own set of instructions. The majority require the engine to be stopped. Read and follow the instructions for the specific feature to ensure expected functionality.

Understanding Advanced Features

Advanced Features provide access to engine information and service functions supported by the connected calibration. Some features help you review operating history; others perform a service action. Read the selected feature's instructions before using its controls.

The features and information available depend on the connected engine calibration. Review the Supported Advanced Features list (PDF) for platform support.

Windows procedure

Open Advanced Features

  1. From the ECM Device Dashboard, select Advanced Features.
  2. Review the Advanced Features screen. It lists features implemented in the Guidanz PC Application and supported by the connected engine calibration.
  3. Select the feature you need to use.

Instructions

Read the selected feature's instructions before using it. The majority of Advanced Features require the engine to be stopped. Follow the instructions for that specific feature to ensure expected functionality.

DTK Mobile differences

Open Advanced Features

In DTK Mobile, from the ECM Device Dashboard, select Advanced Features. The Advanced Features screen displays the supported Advanced Features.

Manage Favorites

Add Advanced Features to the Favorites list to manage the features you use.