Trip Information
Review fuel use, distance traveled, and engine running hours from the connected engine.
Expected result
Trip values for the selected trip type are displayed so you can review fuel consumption, distance traveled, and engine operating time. Only one trip type is displayed at a time.
Understanding Trip Information
Trip Information provides stored engine operating data to help you review engine usage. Use it to understand the operating history represented by the available values.
- Fuel use: The amount of fuel consumed for the period represented by the displayed value.
- Distance traveled: The distance recorded for the period represented by the displayed value.
- Engine running hours: The engine operating time recorded for the period represented by the displayed value.
Review each parameter's name and units when interpreting the values.
Select a trip type
In both DTK Windows and DTK Mobile, use the dropdown near the top of Trip Information to choose which trip type to view. The page displays one selection at a time.
- All Trips (Cumulative): Review cumulative trip data.
- Trips since last reset: Review trip data accumulated since the last reset.
- Trips since last reset engine speed > 0: Review trip data accumulated since the last reset while engine speed was greater than zero.
Windows procedure
- Open Trip Information from the ECM Device Dashboard.
- Use the trip-type dropdown to select the trip data you want to view.
- Expand the available categories to review the values for the selected trip type.
- When authorized or requested, select Reset to reset trip information. Cumulative/lifetime totals are preserved.
DTK Mobile differences
DTK Mobile uses the same navigation, trip-type dropdown, and Reset behavior as DTK Windows. From the ECM Device Dashboard, select Trip Information. Use the dropdown to choose one of the three trip types described above, then review the values for that selection. When authorized or requested, select Reset to reset trip information. Cumulative/lifetime totals are preserved.