Cummins Guidanz DTK
Training home
Work with an engine / Features in Parallel

Features in Parallel

Use multiple supported functions at the same time while connected to a vehicle.

Windows procedure

  1. Connect to the vehicle.
  2. Select the navigation icon in the menu bar.
  3. Use the dropdown menu to open the second desired feature.
  4. Switch between the active features as needed.

Example

You can run a diagnostic test while also creating a Data Monitor recording of engine parameters.

DTK Mobile differences

While connected in DTK Mobile, select the Connection icon at the bottom of the screen. This opens the chyron, where you can select the part of the tool you want to navigate to. Use this control to move between supported features.