Cummins Guidanz DTK
Training home
Diagnostic data / Create a capture file

Create a capture file

Record supported PowerGen controller parameters for later review.

Important notes / prerequisites

When connected to a controller, Capture Files displays only compatible capture files. When no controller is connected, all capture files on the PC are displayed.

Windows procedure

  1. Connect to the controller and open Data Monitor.
  2. Select the required parameter group.
  3. Start recording.
  4. Pause or leave the Data Monitor screen to create the record file.
  5. Review the capture file in the Capture Files view.

DTK Mobile differences

DTK Mobile does not support PowerGen connections. Use DTK Windows for these PowerGen capture-file workflows.

Related Topics

Monitor controller data · Open a capture file · Section overview