Cummins Guidanz DTK
Training homeDiagnostic data / Open a capture file
Open a capture file
Connect to a PowerGen capture file to review its stored parameter values.
Expected result
The selected capture file is connected and its parameter values are available for review.
Important notes / prerequisites
When connected to a controller, Capture Files displays only compatible capture files. When no controller is connected, all capture files on the PC are displayed.
You can connect to multiple capture files and controllers simultaneously.
Windows procedure
- Open the Capture Files add-in.
- Open the three-dot menu for the capture file you want to review.
- Select the option to connect to the selected capture file.
- Review the parameter values within the file.
- When multiple connections are open, select Connection from the toolbar to switch the active connection.
DTK Mobile differences
DTK Mobile does not support PowerGen connections. Use DTK Windows for these PowerGen capture-file workflows.
Related Topics
PowerGen Capture Files · Import or export capture files · Training home