Cummins Guidanz DTK
Training home
Diagnostic data / Import or export capture files

Import or export capture files

Import PowerGen capture files from the local PC and export capture-file data to CSV.

Expected result

Imported capture files are loaded into Guidanz Diagnostic Toolkit. Exporting creates a CSV file, and Guidanz displays its file name and location.

Important notes / prerequisites

When connected to a controller, Capture Files displays only compatible capture files. When no controller is connected, all capture files on the PC are displayed.

Any capture file can be imported. While a controller is connected, an imported file is displayed only if it is compatible with that controller.

Import a capture file

  1. Open the Capture Files add-in.
  2. Select Import File.
  3. Navigate to the capture file on the local PC and select it to load it into Guidanz Diagnostic Toolkit.

Export a capture file

  1. In the Capture Files add-in, open the three-dot menu for the capture file.
  2. Select the option to export the capture file to CSV.
  3. After export completes, review the location and file name displayed by Guidanz.

DTK Mobile differences

DTK Mobile does not support PowerGen connections. Use DTK Windows for these PowerGen capture-file workflows.

Related Topics

PowerGen Capture Files · Open a capture file · Training home