File and storage locations
Locate Guidanz data and exported diagnostic files on Windows and access connection data and logs on DTK Mobile.
Expected result
On Windows, locate the Guidanz storage root and applicable diagnostic-file folder in File Explorer. On DTK Mobile, access the data and logs in the event folder for the connection.
Windows storage root
Guidanz stores data in C:\Users\Public\Documents\Cummins\Guidanz. This location contains folders such as Capture Files and device-specific DT- folders.
Windows procedure
- Open Windows File Explorer.
- Browse to the Guidanz storage root.
- Open the folder for the required data type.
ECM images
ECM images are stored in the work order folder at C:\Users\Public\Documents\Cummins\Guidanz\Events\[Work Order folder]. The work order folder is created during connection to an engine vehicle.
Engine DML recordings
Engine DML recordings are stored in C:\Users\Public\Documents\Cummins\Guidanz\Exports.
PowerGen DML recordings
PowerGen DML recordings are stored in C:\Users\Public\Documents\Cummins\Guidanz\Exports.
Find an exported ECM image
After exporting an ECM image, use the displayed file-location link to locate the exported file. See Export an ECM image for the procedure.
DTK Mobile differences
DTK Mobile: iOS and Android
DTK Mobile runs on iOS and Android. To find data or logs from a connection, use the event folder for that connection in DTK Mobile. The Windows file paths listed above apply to the Windows application.
Find data and logs for a connection
- Identify the connection associated with the data or logs you need.
- Open the event folder for that connection in DTK Mobile.
- Access the required data and logs from that event folder.
When reviewing multiple connections, make sure you open the event folder for the connection you are investigating. All data and logs for that connection should be accessed from its event folder.