Cummins Guidanz DTK
Training home
Home / Configure DTK / User preferences

User preferences

Use Settings & Preferences to manage account profiles, connectivity, application preferences, service information, and troubleshooting options.

Expected result

The selected account, connectivity, notification, display, location, measurement, sleep, locking, and logging preferences are available for the current user.

Important notes / prerequisites

Open Settings from the DTK home screen. The first page is Settings & Preferences. The available options can depend on the signed-in user, platform, equipment, and enabled services.

Settings that apply to the current user are separate from engine or controller settings. Use the applicable equipment workflow when changing device settings.

Windows procedure

  1. From the home screen, select Settings.
  2. Review the Settings & Preferences page.
  3. To manage profiles, select Account Management.
  4. Under Profiles and Accounts, select the user to open User Management. From there, review account status, user initials, device-registration information, subscription management, unit management, PIN changes, or profile removal as applicable.
  5. Return to Settings & Preferences to review other settings.

Settings & Preferences options

User Management

After selecting the user under Profiles and Accounts on the Account Management page, the User Management page can include:

Adding a new user profile logs out the current user but keeps their profile on the device. The new user must create a PIN, just as during the initial login.

Sleep and locking preferences

Service information

Create ECM Image is a single option that enables automatic ECM image creation when connecting to or disconnecting from an ECM. Review this option before starting a diagnostic workflow.

Cummins Guidanz Log File: Select Open the directory to open File Explorer to the folder containing the Guidanz debug log. Send the log directly to a Cummins support team member when they request it for troubleshooting.

Common problems

If an option is unavailable, confirm that you are using the intended user profile and that the applicable service or subscription is available.

If location sharing does not work, enable location on the mobile device or computer and allow Guidanz to use location information.

Enhanced logging captures detailed application logs. Enable it only when requested by Cummins support.

DTK Mobile differences

Settings and Preferences are available on both Windows and Mobile, but the available controls and navigation can differ. Both platforms support notifications when the adapter is out of range or calibrations are complete.