Cummins Guidanz DTK
Training home
Troubleshoot a problem / Non-Supported Engine Programs

Non-Supported Engine Programs

Guidanz Diagnostic Toolkit supports specific Cummins engine programs and communication protocols.

Expected result

The user identifies whether the engine or ECM is supported by DTK.

If unsupported, the user understands which service tool should be used instead.

Important notes / prerequisites

Some older engines, controllers, or equipment configurations may not be supported.

In these situations, another Cummins service tool, such as INSITE, may be required.

Non-supported engine programs and ECMs

Engine programs and ECMs not supported by DTK
Engine ProgramECM
480C-ECM552
B5.9GCM420
C Gas Plus/B Gas PlusCM556
C8.3GCM420
CELECTECM-B
CELECT PlusECM-C
CELECT Plus IndustrialECM-C
CentinelCM400
CENTRYCM400
Gas Compression GTA3.9/5.9/8.3GC, KTA19/38GC - SSM558/CM556/CM2358CM556
SSM558
ISBCM550
ISB - CM850CM850
ISB Daimler ChryslerCM551
ISBe (4 and 6 Cylinder)CM800
ISBe2/3 - CM850CM850
ISBe4 (4 and 6 cylinder)CM850
ISC / Transit Bus ISL8.3 - CM850CM850
ISC/ISLCM554
ISL8.9 - CM850CM850
ISLe4 (6 cylinder)CM850
ISMCM570
ISM - CM870CM870
ISM - CM875CM875
ISM - Fuel Control Module - CM570CM570
KTA19, G855 CM558 G DriveCM558
L Gas PlusCM556
L10GCM420
PIMCM550
QSB5.9/44, 5.9/30, 4.5/30, 3.9/30CM550
QSC8.3/QSL9CM554
CM500
QSK19/23/45/60/78CM500
QSK19G/38G/60G, QSV81/91 - CM700/SSM558/CM2358CM700, SSM558
CM2358
QSM11CM570
QST30CM552
QST30 - Power GenCM552
QSX15CM570
Signature/ISXCM570
Signature/ISX - CM870CM870
K19, K38, & K50 CenturyCM2940

Troubleshooting steps

Step 1: Identify the engine

Determine the engine model and, when available, the Engine Serial Number (ESN).

Step 2: Identify the ECM

Determine the electronic control module installed on the equipment.

Step 3: Verify engine compatibility

Compare the engine program and ECM with the non-supported engine table above.

Step 4: Check communication protocol requirements

Some older engine programs use communication protocols that are not supported by DTK.

Step 5: Use the appropriate service tool

If the engine or ECM is not supported by DTK, use the Cummins service tool recommended for that engine program.

DTK Mobile differences

DTK Mobile and Windows may have different compatibility limitations.

Verify support for the specific DTK platform being used.

Some older engine programs may require a Windows-based service tool.