A calibration will not download
Identify whether the calibration failed to download from Calibration over Web to your PC or mobile device, or failed while being transferred from that device to the ECM.
Expected result
The calibration file is available on the PC or mobile device. For an ECM transfer, the calibration completes successfully and applicable parameters are restored when that option was selected.
Important notes / prerequisites
Important: A successful calibration download does not mean the ECM has been programmed. Follow the applicable calibration installation instructions before proceeding.
If a calibration cannot be downloaded, the issue may involve internet connectivity, calibration availability, access permissions, or temporary server communication problems.
Calibration will not download to the PC or mobile device
Use these checks when downloading a calibration file from Calibration over Web. The retry steps below apply to the file download, before transfer to the ECM begins.
Step 1: Verify internet connectivity
Ensure the device has a stable internet connection.
Calibration files must be downloaded from the appropriate Cummins services.
Step 2: Verify calibration availability
Confirm that the requested calibration is available for the selected ECM.
Not all calibrations are available for every engine or application.
Step 3: Verify user permissions
Ensure your account has the appropriate access to perform calibration-related operations.
Step 4: Check available storage
Verify that sufficient storage space is available to download the calibration file.
Step 5: Retry the download
If the download fails:
- Verify internet connectivity.
- Close and reopen the calibration download screen.
- Retry the download.
If the problem continues, record the error message and contact Cummins Support.
Calibration fails to transfer to the ECM
Use this guidance when the calibration is already on the PC or mobile device, but the ECM programming or recovery process fails.
- Identify the failure stage. Record the exact error message, the ECM identity, and whether the failure occurred during transfer, parameter restoration, or completion.
- Follow the displayed instructions. Calibration transfer can take up to 30 minutes. Maintain sufficient vehicle battery capacity and follow DTK prompts for any required key-off/key-on steps. Loss of power or interruption can leave the vehicle inoperable.
- Use the recovery workflow when offered. After a failed calibration, Guidanz can offer recovery on the next connection. If you select Start Over, DTK returns to Home. Reconnect through Analyze Equipment and use Try Again when offered to attempt recovery.
- Verify completion. Follow Update the calibration to complete the applicable transfer, parameter restoration, and final instructions.
- Escalate an unresolved failure. Preserve the error message, equipment details, and calibration logs. Use Contact Cummins if recovery does not complete.
DTK Mobile differences
Download to the mobile device
DTK Mobile may use Wi-Fi or cellular data to download calibration files.
A stable Wi-Fi connection is recommended when downloading large files.
Ensure sufficient device storage is available.
Keep the application active during the download when possible to reduce the risk of interruption.
ECM transfer and recovery
For supported Mobile calibration recovery, use the same mobile device and user login used for the original calibration download. Recovery choices depend on the stage and type of failure. Follow the displayed prompts and the Mobile calibration and ROM-boot recovery guidance.