Cummins Guidanz DTK
Training homePower generation system / Update the calibration
Update the calibration
Download and install a supported controller calibration package.
Expected result
The controller calibration is updated, and any parameters not restored are identified for follow-up.
Windows procedure
- Open Calibrate Controller from the Device Dashboard or open Calibration Files.
- Use Search Online Calibrations to select a supported controller and download the package to the PC.
- Open the three-dot menu for the desired calibration and begin the process.
- Review the overview and required instructions.
- If Save and Restore is checked, DTK attempts to write custom parameter values back after the base calibration update.
- Review any parameter values that were not restored and write them manually in Device Settings.
Feature files during calibration
During controller calibration, you have the option to select feature files to write to the controller. See Feature Files for downloading, viewing, and writing feature files.
Special calibrations
Special or unavailable calibrations are highlighted after the package is downloaded.
DTK Mobile differences
DTK Mobile does not support PowerGen connections. Use DTK Windows for PowerGen connections and workflows.