Cummins Guidanz DTK
Training homePower generation system / Feature Files
Feature Files
Download feature files with a PowerGen calibration, review downloaded files, and write supported feature files to a connected controller.
Expected result
Downloaded feature files are available for review. When you write selected feature files to a connected controller, their values are written to that controller.
Download feature files
Feature files are downloaded from the cloud when you download the calibration file. See Calibration files for the calibration download workflow.
View downloaded feature files
- From the home page, open Calibration Files.
- Open My Calibrations.
- Select Generators and Power Systems Controllers from the product selector.
- Locate the applicable controller and select View Feature Files.
View and write feature files from the controller
- Connect to the genset controller and open its Device Dashboard.
- Select Feature Files to view the files available for the controller.
- Select the reveal arrow for a feature file to view its parameters and values.
- Select one or more feature-file checkboxes.
- Select Write to Controller when enabled.
Select feature files during calibration
When calibrating a controller, you also have the option to select feature files to write to the controller as part of the calibration workflow.
DTK Mobile differences
DTK Mobile does not support PowerGen connections. Use DTK Windows for PowerGen connections and workflows.