Cummins Guidanz DTK
Training homeDiagnostic data / Create an ECM image
Create an ECM image
Create a snapshot of the controller state for later review, sharing, or analysis.
Expected result
The ECM image is saved and available for later review, analysis, export, or sharing.
Windows procedure
- Connect to the engine and begin Intake.
- During Intake, review the Create ECM Image checkbox and select it to create an image. Its default selection is controlled in Settings.
- Continue through the connection workflow.
- Review the created image in Service History and Files or the applicable device file view.
Create a user-created image while connected
You can create a user-created ECM image during a connected session, in addition to creating an image during Intake.
- Remain connected to the engine.
- On Windows, select the Event icon in the top bar.
- Select Create new ECM Image to create a user-created image.
DTK Mobile
While connected, select Event at the bottom of the screen, then select Create new ECM Image. This provides the same user-created image functionality as Windows.
Image contents
ECM images include Faults, Device Settings, and Audit Trail information available when the image is created.