Cummins Guidanz DTK
Training home
Power generation system / Perform commissioning

Perform commissioning

Use Commissioning to set up a new genset with grouped controller settings.

Expected result

The selected commissioning workflow completes and the required controller settings are saved.

Important notes / prerequisites

Commissioning is intended for bringing a new genset online. The supported commissioning areas are OEM, IO, and Paralleling.

Windows procedure

  1. Connect to the controller and open the Device Dashboard.
  2. Select Commissioning.
  3. Select the required commissioning area.
  4. Complete the OEM, IO, or Paralleling workflow as applicable.
  5. Review and save the required settings.

DTK Mobile differences

DTK Mobile does not support PowerGen connections. Use DTK Windows for PowerGen connections and workflows.