Cummins Guidanz DTK
Training home
Diagnostic data / Use a template

Use a template

Write a saved template to an ECM to apply multiple predetermined device settings.

Expected result

The selected template values are written to the ECM and the result is available for verification.

Important notes / prerequisites

Templates reduce manual configuration by writing multiple supported settings in one operation. Only write values that are authorized for the connected equipment.

Windows and Mobile procedure

  1. Open the Templates page.
  2. Select the saved template and review its values.
  3. Select Write to ECM.
  4. Follow the connection and confirmation steps.
  5. Review the result and verify the values on the ECM when required.

DTK Mobile differences

DTK Mobile follows the same procedure as DTK Windows for using a template. Follow the Windows and Mobile procedure above.