Cummins Guidanz DTK
Training homeDiagnostic data / PowerGen Capture Files / Overlay a capture file
Overlay a capture file
Write all or selected capture-file parameters to a connected PowerGen controller.
Expected result
The selected parameters are overlaid into the controller. Parameters that could not be written are highlighted after the process completes.
Important notes / prerequisites
When connected to a controller, Capture Files displays only compatible capture files. When no controller is connected, all capture files on the PC are displayed.
Connect to the target controller and select a compatible capture file before starting an overlay.
Overlay a capture file into a controller
- Connect to the target controller and open Capture Files.
- Open the three-dot menu for the compatible capture file and select Overlay file into controller.
- Choose to write all parameters or use the partial overlay option to select individual configurable parameters.
- For a partial overlay, select or clear the checkboxes for individual parameters or entire groups.
- After selecting the features and parameters to overlay, select Continue.
- After the overlay completes, review the parameters that could not be written to the controller.
Parameters that fail to write are highlighted after the process completes.
DTK Mobile differences
DTK Mobile does not support PowerGen connections. Use DTK Windows for these PowerGen capture-file workflows.