Cummins Care - Electronic Service Tools

INCAL

 

If your vehicle has an OEM engine installed from Case New Holland (CNH), the calibration files are NOT available from Quickserve Online (QSOL). Please check following text file for the calibration files, if they are listed, you will need to use the version of Insite bundled with the CNH Electronic Service Tool (EST). If you are not a CNH dealer, consult your nearest CNH dealer.  Click Here for Calibration Details

 


INCAL Download

Before You Attempt to Download

Before Downloading these ISO's you might want to check your networks bandwidth to see if it can handle downloading these large files. You can test your network speed at http://www.speedtest.net/ 

Downloading a 7 Gb ISO will take time based off your connection speed below. The download time is in Hours:Minutes:Seconds

Connection type Download speed Download time
Modem 28,8 kbit/s
Modem 56,6 kbit/s
ADSL 256 kbit/s
ADSL 512 kbit/s
ADSL 1 Mbit/s
ADSL 2 Mbit/s
ADSL 8 Mbit/s
ADSL 24 Mbit/s
LAN 10 Mbit/s
LAN 100 Mbit/s
Turbo 3G 7,2 Mbit/s
4G 80 Mbit/s

Note that transfer rates are quoted as binary values (i.e. 1 Mbps = 1024 Kbps). Also note the difference between the case of the "b" - "-bps" means bits per second and "-Bps" means Bytes per second. For data quantity, you may choose between binary (e.g. MiB) or decimal (e.g. MB) versions of units.
For reference, typical modem speed is 56 kbps and broadband connection may range from 128 kbps to 25 Mbps (although it is normally in the 1-5 Mbps range).

 

August 2017 INCAL DVD Set (Updated Every Two Months)

Aftertreatment Doser
Calibration Database Only
Aftertreatment_Doser.zip Size: 2 Mb
This Database will expire on:
Sunday, September 3, 2017
Engine Fuel Supply Pump
Calibration Database Only
Engine_Fuel_Supply_Pump.zip Size: 568 Kb
This Database will expire on:
Sunday, September 3, 2017
Turbo Actuator Controller
Calibration Database Only
Turbo_Actuator_Controller.zip  Size: 2 Mb
This Database will expire on:
Sunday, September 3, 2017
 
Disk 1 DVD Download  Size: 6.9 Gb INCAL DVD Cover Letter and DVD Details
August 2017 INCAL DVD Cover Letter rev1.pdf Size: 80 Kb
Disk 2 DVD Download Size: 7.5 Gb
Disk 3 DVD Download Size: 7.0 Gb

 

SIR DVD (Updated Quarterly)

Disk 1 DVD Download
Disk Size: 7 Gb
  DVD Details

 

RMI DVD (Update Quarterly)

Disk 1 DVD Download
Disk Size: 302 Mb
DVD Details