Cummins Care - Electronic Service Tools

INLINE 7, INLINE 6, & INLINE 5 Driver Downloads

INLINE 7 Software Download  (Part Number: 5299899 )
The INLINE 7 driver below works on both 32bit and 64bit machines.

 

cummins-inline-7-software-download-button Version 2.3.0.0

INLINE 6 Software Download (Part Number: 2892092 )
Note that if you have an INLINE 6 adapter, you must install the INLINE 6 PC Driver that is included in this software. The INLINE 6 Software installation is a typical Windows-based, self-executing installation. Version 6.4.1.0 of the executable setup file installs the latest INLINE 6 PC Driver, which allows RP1210-compatible software applications to communicate with the INLINE 6 adapter. The latest version of the reflash utility and version 6.41 of the firmware are also included in this download and will be installed automatically in their proper folders in your PC when you run the install program, as described below.

INLINE 6 (32-bit)

INLINE 6 (64-bit)

Reflash Instructions - INLINE 6

  1. Download the appropriate INLINE 6 zip file by clicking on a link above (note that unless you have a 64-bit Operating System, you should use the 32-bit file).

  2. Unzip and extract the executable file using zip/unzip software.

  3. Click on the Windows Start menu and click Run.

  4. Click on the Browse button and locate the file you have downloaded.

  5. Click the OK button to install the latest INLINE 6 Driver, reflash utility, and firmware on your PC.

  6. Follow the onscreen instructions to complete the installation.

  7. Connect +8 V to +50 V power to your INLINE 6 adapter through the DB25 cable you have.

  8. Use your DB9F to DB9M serial cable or USB cable to connect the INLINE 6 adapter to the proper PC communication port.

  9. Follow the Driver Installation and other instructions located on the On-line Manuals page.


INLINE 5 Software Download (Part Number: No Longer Available)
Note that if you have an INLINE 5 or INLINE 4 adapter, you must install the proper INLINE 5 PC Driver that is included in this software. The INLINE 5 Software installation is a typical Windows-based, self-executing installation. Version 5.6.5.4 of the executable setup file installs the latest released INLINE 5 PC Driver, which allows RP1210-compatible software applications to communicate with the INLINE 5 adapter. The latest version of the reflash utility and version 5.46 of the firmware are also included in this download and will be installed automatically in their proper folders in your PC when you run the install program, as described below. Note that if you have issues with a DEF gauge, you should use Driver Version 5.7.0.1. which has version 5.47 of the firmware.

INLINE 5 (32-bit)

INLINE 5 (64-bit)

Instructions for Downloading INLINE 5

  1. Download the appropriate INLINE 5 zip file by clicking on a link above (note that unless you have a 64-bit Operating System, you should use the 32-bit file).

  2. Unzip and extract the executable file using zip/unzip software.

  3. Click on the Windows Start menu and click Run.

  4. Click on the Browse button and locate the files you have downloaded. (Use version 5.6.5.4, unless you have DEF gauge problems, in which case you should use 5.7.0.1).

  5. Click the OK button to install the correct INLINE 5 Driver, reflash utility, and firmware on your PC.

  6. Follow the onscreen instructions to complete the installation.

  7. Connect +8 V to +50 V power to your INLINE 5 adapter through the DB25 cable you have.

  8. Use your DB9F to DB9M serial cable or USB cable to connect the INLINE 5 adapter to the proper PC communication port.

  9. Follow the Driver Installation and other instructions located on the On-line Manuals page.