Cummins Care - Electronic Service Tools

Cummins Guidanz

To diagnose, repair and update the Route Parameter Manager in your Cummins ADEPT™ equipped truck, you will need to download copy of Cummins Guidanz™ for your Android phone or tablet, or for iPhone and iPad. 

  Click to Enlarge QR Code

  Click to Enlarge QR Code

Datalink Adapter Information for Guidanz™

To use Guidanz™ you will need one of the new Cummins wireless datalink adapters. 

  

INLINE™ 7 is a complete kit, with 9, 6 and 3 pin cables to connect to equipment. It supports USB, WiFi, and Bluetooth so works on INSITE as well as Cummins Guidanz™

  

INLINE™ mini is an inexpensive, palm-sized, Bluetooth adapter with no need for additional cables, designed especially for Guidanz™

 For more information, or to purchase Cummins datalink adapters, visit CumminsEngines.com/INLINE

 

Downloading the Map Files

Version Number Release Date Description File Name
3692961.01 September 15, 2016 North America ADAS 2015 3692961_01.zip

1. Get a USB thumb drive. Make sure there are no other files, and especially no previous map files or folders on the drive.

2. Download the latest map file, unzip it, and move the eHorizon_Map folder to the USB thumb drive.

3. Make sure you place the "eHorizon_Map" folder is in the lowest level (root directory) of the thumb drive. Do not put it inside any subfolders or the module will not be able to find the files. 

 

Installing the Map Files

Once maps are on the USB thumb drive, plug it into the end of the USB cable attached to the Route Parameter Manager module. If the cable is missing or damaged, a replacement one can be ordered as Cummins Part #5394154 from your authorized dealer or distributor.  

Attach your INLINE data link adapter, launch Guidanz and connect to the Route Parameter Manager module. Several functions are available, but select the Update RPM Maps function and follow the on-screen instructions.  

Troubleshooting

If you cannot connect to the Route Parameter Manager, there may be a bus configuration issue. Some engine configurations require that Cummins Parameter Manager hardware be installed in order to access the module for service. Please refer to TSB150099 for the complete product list and compatibility charts.   

If you have issues getting the Route Parameter Manager module to read the map files, or recognize the thumb drive at all: ·        

Cummins ADEPT

ADEPT™ is a suite of advanced electronic features for the ISX15 engine that interact with automated manual transmissions, dynamically adapting to operating conditions to help even novice drivers operate as efficiently as your most seasoned and efficient professional. ADEPT enhances fuel economy with no impact to productivity, harnessing the electronic capabilities of the engine and transmission to make powertrain control decisions in real time.   The Route Parameter Manager module uses GPS and a set of onboard maps to preview the road ahead so it can adjust engine and transmission settings to improve the fuel economy of your truck. Learn more about how Cummins ADEPT can help improve your driving efficiency.